Page 3 of 4 FirstFirst 1234 LastLast
Results 21 to 30 of 34

Thread: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

  1. #21
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    122
    Images
    1
    Rep Power
    15

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Quote Originally Posted by jwatte View Post
    www.saleae.com

    The cheapest one (Logic 4, $109) will probably be just barely enough. I've upgraded my way through their offerings (started at the bottom many years ago) and am now on the 16 Pro.
    You can probably live with the second-cheapest (Logic 8, $219) for a very long time, especially these days when it also comes with analog input. (Used to be digital-only.)
    Up vote!

  2. #22

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Quote Originally Posted by m3atsauc3 View Post
    https://www.sparkfun.com/products/13929
    Anyone used one of these?
    Nope, Looked somewhat interesting. I Have not advanced as far as jwatte

    I started off with one of their first ones that I later gave away, I upgraded to the 16 channel one when it came out. I then supported their sort-of kickstarter for the new ones and purchased the Logic-8. Later when I wanted to debug some higher speed interfaces, I purchased the Pro8... So right now I have all three of them on my Desk as I am debugging some new implementations of the SPI library for the Teensy boards and so I am testing things out on T3.6, 3.5, 3.2, T-LC and a little with T2... And it is nice to be able to switch between the different boards ana have some of them already setup to LA...

    If I were to choose one for beginner/Intermediate usage, I would probably suggest the Logic 8, unless you are only doing simple things.
    For example with the SPI stuff, I am doing some testing using things like an SSD1306 display and it is nice to hook up the Logic analyzer to see (MOSI, MISO, SCK, CS, DataCommand) which you can not do all of them on the Logic 4... It is only rare times when I need more than 8, but used it last week again testing with the Async SPI code where I was testing on T3.5 or 3.6 with three of these displays, one on each SPI buss and I wanted to see how well all of the SPI signals were being done concurrently... Sorry for the regression...

    (Now in process of debugging Async 16 bit writes using DMA on T3.6...

    P.S - I also have a custom Analyzer that R3n33 started for the AX messages which is nice to use.

  3. #23

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    That one looks new! No, I have not used it.
    If you try it out, let us know how it works!

  4. #24

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    It's been a while, but the project is still ongoing! Here's a bit of progress news:
    I have sourced most of the metal and plastic brackets and motors. I did not have enough of the standard plastic brackets, and they seemed to be out of stock online, so I decided to get them some printed by Shapeways.
    For now I should be able to put together 2 front legs and spine, using some temporary brackets for the body. Later on there will be various 3D printed parts, both structural and decorative.
    I've decided to go with an all-blue colour scheme, so the 3d Printed parts were done in the Shapeways standard blue. I tried spray-painting the metal brackets as well as the small plastic washers/bushings, and they haven't come out too bad. I guess the spray paint will chip/come off over time, but I'm not too concerned, if anything it will give it a seasoned look!
    On the software side, some of the kinematics code has been ported to the Arbotix, while I'm also working on some fixed walking gait patterns which will let the quad make its first steps.

    Images:
    Click image for larger version. 

Name:	IMG_20170922_192952.jpg 
Views:	211 
Size:	106.8 KB 
ID:	7084Click image for larger version. 

Name:	IMG_20171008_211126.jpg 
Views:	194 
Size:	145.8 KB 
ID:	7091Click image for larger version. 

Name:	IMG_20171005_194607.jpg 
Views:	190 
Size:	142.7 KB 
ID:	7085Click image for larger version. 

Name:	IMG_20171006_073850.jpg 
Views:	186 
Size:	117.1 KB 
ID:	7086Click image for larger version. 

Name:	IMG_20171006_073948.jpg 
Views:	185 
Size:	151.7 KB 
ID:	7087
    Click image for larger version. 

Name:	IMG_20171008_180859.jpg 
Views:	188 
Size:	149.4 KB 
ID:	7088Click image for larger version. 

Name:	IMG_20171008_200700.jpg 
Views:	190 
Size:	126.9 KB 
ID:	7089
    Click image for larger version. 

Name:	testQuadGait.jpg 
Views:	187 
Size:	64.6 KB 
ID:	7090

  5. #25

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Two legs built and old test rig scaffold repurposed. Videos to follow soon hopefully.

    Click image for larger version. 

Name:	IMG_20171018_203133.jpg 
Views:	208 
Size:	175.9 KB 
ID:	7094

  6. #26

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Looks neat!

    I'll be super interested in seeing how it turns without a yaw servo but instead having two roll servos. While you're moving dynamically, that might enable some cool gaits.

  7. #27

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    I've managed to get all the motors now, and assembled all the legs!

    The walking is very crude at the moment, as it's just using a test walking gait sequence from the test program converted directly to motor position commands via serial. The quad doesn't really maintain its balance, hence the helping hand.

    The current chassis is temporary, using MakerBeam aluminium profiles, so the next stage is to start building the CAD modelled chassis, out of aluminium sheets and 3D parts, then focusing on getting more effective walking gaits.


    My first attempt at putting some effort into editing a video (it's very time-consuming!):
    https://www.youtube.com/watch?v=Bc8oe3zt6aA


    Click image for larger version. 

Name:	IMG_3521.jpg 
Views:	193 
Size:	75.7 KB 
ID:	7108

    Click image for larger version. 

Name:	IMG_3546.jpg 
Views:	177 
Size:	92.3 KB 
ID:	7109
    Click image for larger version. 

Name:	IMG_3532.jpg 
Views:	169 
Size:	61.4 KB 
ID:	7110
    Click image for larger version. 

Name:	IMG_3530.jpg 
Views:	190 
Size:	70.4 KB 
ID:	7111

    Snow is very rare here, so it was a nice chance for some photos in the wild!

  8. #28

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    After lots of 3D printing and some metalwork, this is the current state of the chassis:

    Click image for larger version. 

Name:	IMG_20180201_202407.jpg 
Views:	188 
Size:	104.3 KB 
ID:	7151 Click image for larger version. 

Name:	IMG_20180201_210312.jpg 
Views:	181 
Size:	122.4 KB 
ID:	7152 Click image for larger version. 

Name:	IMG_20180201_224347.jpg 
Views:	183 
Size:	142.6 KB 
ID:	7153

    There's a lot of weight for those middle servos and brackets to handle, so may need a slight design change ...

  9. #29

    Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Yeah, weight is the bane of all walkers ...

  10. Re: Quadbot 17 - Quadruped robot designed in Autodesk Fusion 360

    Hi

    The bot looks great! Are you still working on it? I am researching a build for a quadruped using just 3dof legs and looked at the AX12A servos. How did you get on with them? Did they seem up to the task, or did they top out fairly quickly? I would like to keep the costs down and the AX18's have a ton more grunt, but for twice the price!

    Cheers

    Wire

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How to do the fine calibration of a Quadbot using Phoenix Code
    By punyviking in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 09-29-2016, 01:12 PM
  2. Kinect Fusion
    By billyzelsnack in forum Robotics General Discussion
    Replies: 1
    Last Post: 08-12-2011, 12:23 AM
  3. Contest Entry Fusion
    By Quantum in forum Project Showcase
    Replies: 4
    Last Post: 10-25-2010, 11:53 PM
  4. Alum Robot Quadruped custom kit
    By innerbreed in forum Garage Sale
    Replies: 0
    Last Post: 10-17-2009, 08:26 PM
  5. News/Announcement Autodesk Student Community - Free Autodesk Software
    By srobot in forum Software and Programming
    Replies: 16
    Last Post: 10-15-2008, 03:20 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •