Results 1 to 8 of 8

Thread: 3D Printer Knowlege and advice for upgrading

  1. #1
    smith59 Guest

    3D Printer Knowlege and advice for upgrading

    Not sure if it is best to start a new conversation or continue here. so...


    I am also thinking about jumping in and getting a 3d printer, so that I can at first print up some of the different parts for the HROS1 and for my PhantomXs. But not sure which one would be a good one to purchase for a first time printer...


    For starters lets say for under 1000. If however it turns out that there is one for $1200 that is so vastly superior than...


    Example a lot of reviews appear to like: http://www.3dprintmanual.com/best-cheap-3d-printers/


    I am assuming a heated bed, sort of like the idea of being in an enclosure. Assume it supports PLA. Nice if was not totally restricted to vendors materials only, but not a deal breaker. My guess something like 8x8x8 would be great... single extrusion would probably work to learn with...


    I see lots of different lists and reviews like: http://www.3dprintmanual.com/best-3d-printer-filament/
    But hard to know which to trust.




    or maybe something like: http://www.3dprintmanual.com/best-3d-modeling-software/


    Suggestions?

  2. #2

    Re: 3D Printer Knowlege and advice for upgrading

    A heated bed and enclosure is only needed for certain materials. I've printed PLA for years without heated bed and without enclosure, and it works great!
    I recommend the Printrbot Simple Metal: http://amzn.to/2mnvUKl
    It's $500 without the heated bed, $650 with, both come assembled and ready to print once you unpack and set them up!

  3. #3
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    87

    Re: 3D Printer Knowlege and advice for upgrading

    I'm not a 3D printer expert. It all depends what you plan to use it for. But I would definitely recommend a heated platform if you plan to use other materials than PLA. You can easily build your own enclosure/cabin later. If you need stronger and more durable parts ABS is a great material, but you need good ventilation. Then again other materials like PETG is more environmental friendly.

    The latest Prusa i3 MKII printer looks great and Fusion 360 is a great CAD program.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  4. #4

    Thumbs up Re: 3D Printer Knowlege and advice for upgrading

    Quote Originally Posted by Zenta View Post

    The latest Prusa i3 MKII printer looks great and Fusion 360 is a great CAD program.
    Think thats a great start!
    I have a Ultimaker orginal +, but a prusa is at my wish list
    I chose a bowden printer cause i read it could print faster, but i dont use high speed settings as often.
    Direct drive gives better extrution, especially for soft filaments.
    I like the heated bed. After i discovered the plastidip spray on sand blasted glass bed, I only use the heated bed just for other materials then PLA

    And Fusion360 is awesome!!

    First post

  5. #5

    Re: 3D Printer Knowlege and advice for upgrading

    I need to get back to my 3d printer and print some stuff out... Maybe print out a Chip-E...

    In case anyone is interested, there is a pretty cheap printer being done on Kickstarter.
    https://www.kickstarter.com/projects...in/description

  6. #6
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: 3D Printer Knowlege and advice for upgrading

    Quote Originally Posted by KurtEck View Post
    In case anyone is interested, there is a pretty cheap printer being done on Kickstarter.
    https://www.kickstarter.com/projects...in/description
    Which I'm in for a Deluxe (PEI heated bed and OLED screen) with filament detector and single extruder. Gonna make me some gearboxes, LED PCB holders, and a bigger, sturdier, faster printer with volcano-size hardened steel nozzle (and possibly a cast SiO2 thermal break in the hot-end).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  7. #7

    Re: 3D Printer Knowlege and advice for upgrading

    Hi Tician,

    I ended up ordering about the same setup as you mentioned (I am in the October batch). So far I have not added the filament detector. I still have the other printer but thought that when I am busy trying to print something there are times i need multiple.

    Looks like it turned into a popular Kickstarter as their goal was $100K, and they are now over $600K, which unlocked some new stretch goals/rewards, like now it will include a cooling fan... Also now have option $50 for dual extruder.

    Edit: I decided add the filament detector...
    Last edited by KurtEck; 06-19-2017 at 12:29 PM.

  8. #8

    Re: 3D Printer Knowlege and advice for upgrading

    What I learned yesterday: If you print a thing with good dimensions in PLA, and then let it sit in a hot car for a week, it will shrink by a significant amount!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. 3D Printer Knowlege and advice for upgrading
    By Amp in forum Robotics General Discussion
    Replies: 29
    Last Post: 11-25-2015, 04:43 AM
  2. A DIY DLP Resin 3-D printer
    By Gort in forum Project Showcase
    Replies: 5
    Last Post: 07-07-2013, 04:03 PM
  3. 3D Printer recommendations
    By AVRnj in forum Robotics General Discussion
    Replies: 44
    Last Post: 04-13-2013, 12:42 PM
  4. For Sale --> New Printrbot 3D Printer
    By Scope in forum Garage Sale
    Replies: 3
    Last Post: 01-19-2013, 04:07 PM
  5. 3D Printer
    By Robonaut in forum Off Topic
    Replies: 2
    Last Post: 05-24-2011, 09:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •