Page 1 of 3 123 LastLast
Results 1 to 10 of 30

Thread: 2017 Robogames Mech Warfare Qualifying

  1. #1
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    189
    Rep Power
    21

    2017 Robogames Mech Warfare Qualifying

    Click image for larger version. 

Name:	RTeam Logo.jpg 
Views:	183 
Size:	11.1 KB 
ID:	6914
    http://rteamrobotics.weebly.com/

    Post qualifying videos for the 2017 Robogames Mech Warfare Event here.

    Videos should be 5 minutes long and demonstrate you can hit targets and have mobility for the entirety. They can be video'd in whatever space you have available... kitchen floor, garage, outdoors, etc...

    Here's the running list of the Pre-Qualifiied Mechs:
    1) Apophis
    2) Nomad
    3) Odin
    4) '99
    5) Obsidian
    6) Onyx
    7) Domino
    8) Daisy
    Last edited by GhengisDhon; 04-21-2017 at 08:55 AM.

  2. #2
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    189
    Rep Power
    21

    Re: 2017 Robogames Mech Warfare Qualifying

    Apophis

  3. #3
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    189
    Rep Power
    21

    Re: 2017 Robogames Mech Warfare Qualifying

    Nomad

  4. #4
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    189
    Rep Power
    21

    Re: 2017 Robogames Mech Warfare Qualifying

    Odin

  5. #5
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    189
    Rep Power
    21

    Re: 2017 Robogames Mech Warfare Qualifying

    '99

  6. #6

    Re: 2017 Robogames Mech Warfare Qualifying

    Apophis Qual FPV Perspective


    Nomad Qual FPV Perspective


    Odin Qual FPV Perspective


    Mech 99 Qual FPV Perspective

  7. #7

    Re: 2017 Robogames Mech Warfare Qualifying

    The FPV sound of '99 is awesome! The walking distorts enough to be a nice "crunch" for footsteps. and the firing is a authentic-sounding beep-SMACK!

  8. #8
    Join Date
    May 2016
    Location
    White Plains, NY
    Posts
    122
    Images
    1
    Rep Power
    9

    Re: 2017 Robogames Mech Warfare Qualifying

    I love these videos! And I have 13 months to get one ready myself! I have two questions:

    1) Has anyone implemented non-linear aiming? Such that the servo response is small with small joystick deflection, and larger with large deflections? In the videos I see folks struggling to make small movements. This is the kind of thing that's very easy to implement in software

    2) Has anyone considered gyro-stabilized turrets? I would think I would be almost unbeatable if I could move and fire at the same time, and a stabilized gun should make this pretty easy.

    Just thinking aloud!

  9. #9

    Re: 2017 Robogames Mech Warfare Qualifying

    Has anyone implemented non-linear aiming?
    The main problem is that the servos have limited resolution. 1024 steps over 300 degrees means about 0.3 degrees per step. Add backlash and the inherent flex in thin (lightweight) construction, and it's harder than it seems! (The MX series gets you 4096 steps over 360 degrees, so slightly better.)

    I've seen some people try to use lever or pushrod based designs (the new Numa in the other thread seems like one?) but don't know how well that works. With the right design, it should give you better precision; don't know what it does for backlash and flex.

    Has anyone considered gyro-stabilized turrets?
    Josh Pieper did this last fall. Walking while shooting. There's still jerking when moving, as far as I can tell, and there was some other hardware issue that prevented him from doing really well IIRC. You may be able to find the thread if you look for the Phoenix robo meetup.

    For gyro stabilization, the servos are too slow to do a good job, so you need to go with drone flyer FPV style gimbals. These use brushless DC motors with direct drive, and glue the sensor onto the actual gimball. There's a question of payload capacity, because the lighter-weight gimbals are for cameras in the 100 gram weight class, and gun + camera + ammo weighs more than that. (The tube-based ammo feeders may help here.)
    There's also the problem that a gimbal can't stabilize very well when there is lateral (translation) motion which there is a fair bit of when walking.
    It's still a great idea, and I have some designs myself to that effect, but the main problem is always time or cost -- for students, cost; for employed engineers, time :-)

  10. #10

    Re: 2017 Robogames Mech Warfare Qualifying

    Quote Originally Posted by jwatte View Post
    Josh Pieper did this last fall. Walking while shooting. There's still jerking when moving, as far as I can tell, and there was some other hardware issue that prevented him from doing really well IIRC. You may be able to find the thread if you look for the Phoenix robo meetup.
    Our turret worked great, we had some problems with the USB on our processor board cutting out. With our wifi and video over USB, when it cut out, it was end of match. That said, overall it worked well enough to place third.

    http://joshp.no-ip.com:8080/blog/rob...ed-turret.html

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. 2017 Robogames Mech Warfare Attendance Survey
    By GhengisDhon in forum Mech Warfare
    Replies: 21
    Last Post: 04-19-2017, 11:06 PM
  2. Mech Warfare Scoring Transponder 2017
    By artans in forum Mech Warfare
    Replies: 33
    Last Post: 04-16-2017, 12:57 AM
  3. Robogames 2017 Mech Warfare Ruleset
    By giantflaw in forum Mech Warfare
    Replies: 34
    Last Post: 03-25-2017, 02:43 PM
  4. 2016 Robogames Mech Warfare Qualifying
    By GhengisDhon in forum Mech Warfare
    Replies: 19
    Last Post: 04-10-2016, 12:39 PM
  5. Will there be Mech Warfare for Robogames 2012?
    By bloftin in forum Mech Warfare
    Replies: 2
    Last Post: 02-26-2012, 11:06 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •