Page 1 of 2 12 LastLast
Results 1 to 10 of 15

Thread: General Grievous

  1. #1
    Join Date
    Mar 2010
    Location
    Stavanger, Norway
    Posts
    7
    Rep Power
    36

    General Grievous

    Its been around 10 years since I purchased my Robonova-1, after playing around with it for while before a house purchase took over all my spare time. Back in summer of 2015 I changed my job and I felt it was time to get back into robotics. After a lot of searching and "window-shopping" on the internet, I decided to give the old Robonova a new approach to see if the interest and time was there without investing to much money. I did some mechanical changes to the bot to make it more similar to the DARwIn-OP. After a while I figured out that time had run out for the Hitech servos and abandoned the whole project. I had my eye on the HR-OS5, but at a price tag of $20 000 it was a pretty hefty investment, and I spent half a year playing around in SolidWorks and ROS before I did my first purchase, which was six MX-64AT and frames for the upper body:

    Click image for larger version. 

Name:	20161019_211127-cropped.jpg 
Views:	671 
Size:	100.3 KB 
ID:	6920

    I had an accident with the Arbotix Pro controller, breaking of the micro usb connector. It's not pretty, but I fixed it with some soldering and using the Molex connector instead.
    Click image for larger version. 

Name:	20161018_084836-cropped.jpg 
Views:	647 
Size:	98.3 KB 
ID:	6921

    Got around and ordering the rest of the parts arriving mid February 2017
    Click image for larger version. 

Name:	20170213_175845-cropped.jpg 
Views:	656 
Size:	69.9 KB 
ID:	6922Click image for larger version. 

Name:	20170213_175959-cropped.jpg 
Views:	638 
Size:	57.1 KB 
ID:	6923

    My idea is to make this a ROS "powered" bot, and in addition to the HR-OS5 I have added two extra DOF in each arm, including a gripper.
    Click image for larger version. 

Name:	20170213_211432-cropped.jpg 
Views:	654 
Size:	132.9 KB 
ID:	6924
    I'm not 100% satisfied with the add-on design, and I want to use the available HR-OS5 framework by interbotix, I'll take it of until the base configuration is ready.

    I've always been a StarWars fan, so I also want to try to make the bot look like General Grievous. This is not a main priority at the moment, but I'll at least stick with the name!
    Click image for larger version. 

Name:	general_grievous_remaster_by_oblivionhunter1-d976p10.jpg 
Views:	672 
Size:	61.4 KB 
ID:	6926
    Last edited by Pengatom; 03-24-2017 at 10:12 AM.

  2. #2

    Re: General Grievous

    You're writing all that, and we don't get to see a picture? That counts as teasing :-)
    It sounds like you're making progress, and by all means, I look forward to seeing updates!

  3. #3
    Join Date
    Mar 2010
    Location
    Stavanger, Norway
    Posts
    7
    Rep Power
    36

    Re: General Grievous

    Quote Originally Posted by jwatte View Post
    You're writing all that, and we don't get to see a picture? That counts as teasing :-)
    It sounds like you're making progress, and by all means, I look forward to seeing updates!
    I've added some pictures and updated the first post. Planning on future updates to the first post and some comments (hopefully from someone else than myself) and progress in future posts.

    I have put most of my effort in assembling the robot and updating the assembly document while building. The main bot is now completed, except for the head and the grippers. I forgot to order the idle bearings for the MX-28 when I put in the big order back in January, and now I've been travelling with work for the last month first Houston and these days in Singapore. I order all parts needed to complete the head and grippers back in March, so when I come back home I have to get all designed parts 3D printed and I'll be able to complete the whole bot.

    Mechanically that is, I still need to finish up everything related to power supply. For now the servos are running off the 12v10a SMPS power supply and the NUC is using its original power supply, so I need to look into batteries and wiring everything together. I'd really like to have some schematics on how this is done, which input is used for the NUC for instance. I'm playing around an idea to add a On-Off-On switch between the NUC and the main power so I have the option of powering it either from batteries or the power supply, but I would really like to have possibility to power it from a external power supply while the batteries are charging without the need of powering down either planned or unexpectedly...

  4. #4

    Re: General Grievous

    Love the pictures! Looks like a fun project.
    Personally I'd prefer to read updates in additional comments, rather than an updated first post. (Although adding the pictures was swell :-)

    You can make the power supply powering the robot be automatic by adding a diode. When both battery and power supply is connected, if battery voltage is less than (12.0V - Vf_diode) then the battery will be charged by the power supply. For a Schottky power diode, you'll see about 0.6V drop, so it'll be about 11.4V battery float voltage.
    I find that keeping the power supply in parallel with the battery is the best of both worlds, because the battery is there for the large current spikes when things start up or move strenuously, whereas the power supply makes sure I never run low on battery and can keep it on indefinitely while developing.

    If you use a power supply with a current limit (rather than hiccup mode) and with adjustable voltage, you don't even need the diode, as long as you unplug the power supply when you turn if off to avoid draining the battery through the PS output. Typical "bench" power supplies work well for this.

  5. #5
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    85

    Re: General Grievous

    Good to see you having some progress with your project!
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  6. #6
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    93

    Re: General Grievous

    On Golem i use a voltage up-converter to 19v to power the NUC. This allowed me to stick with 3cell Lipos. Works fine the past two year without problems.

  7. #7
    Join Date
    Mar 2010
    Location
    Stavanger, Norway
    Posts
    7
    Rep Power
    36

    Re: General Grievous

    Appreciate the comments!

    Was thinking of updating the first post to make it more of a overall presentation of the bot, duplicate/addition to whatever happens throughout this thread.

    Regarding power, the HR-OS5 is designed with dual 2cell LiPo for better balance and I think I'll keep this feature. This will give me 14.8V to work with and according to the specs the NUC can be powered either with 12-24v to the internal connector or 12-19 on the external connector and the Arbotix Pro takes 12-24v input so I don't really think I need to step up the voltage to 19, unless I'm missing something?

    Now, for parallell powering, since I'm gonna use LiPo batteries, wouldn't that cause an issue if I try to charge two 2s batteries connected in series with my 12v power supply? My impression is that LiPo's are somewhat unstable and should be removed and charged separately under close supervision. This is a issue that I've been very unsure on how to deal with in the best way, so any input here is highly appreciated

  8. #8
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: General Grievous

    Very strongly recommend you use 3S LiPo until you have a working gait as a fully charged 4S LiPo will be almost 17V, which will cause overvoltage alarms on the MX servos until the battery voltage drops below 14.8V. While the specs state that MX servos can handle up to 14.8V, they will experience higher rates of damage/failure at any voltage over 12V during any collision, stalling, overloading, etc. Using a 3S LiPo will also permit using a 12V power supply, which would not be otherwise practical as 12.8V is dangerously drained for a 4S LiPo.

    If you must have the higher voltage battery, then 4S LiFePO4 is a safer choice than 4S LiPo given the fully charged voltage of ~14.4V and nominal voltage of ~13V. LiFePO4 is also much more tolerant of abuse during both charge and discharge. The big problem is that the series connected cells tend to become unbalanced much faster than LiPo, so will have to perform a proper balance charge much more often if normally performing a quick charge.

    A 3S LiPo has a nominal voltage of 11.1V which will likely cause undervoltage alarms on a NUC without a 19V boost converter. The higher performance consumer systems I own are even less tolerant regarding the input voltage and absolutely require a 18~20V supply or they will beep incessantly and refuse to boot.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  9. #9
    Join Date
    Mar 2010
    Location
    Stavanger, Norway
    Posts
    7
    Rep Power
    36

    Re: General Grievous

    Ok, so its better to use a lower voltage source and step up the voltage for the NUC than to use a higher voltage and limit it for the servos? I'm pretty new to these kinds of batteries, only batteries I have is NI-MH, so its a different ballgame altogether.

    Also, this is the setup which is sold by Trossen, wouldn't this be things they thought of? I' just curious, and want to know as much as possible to do the right choice here before spending money on batteries and electronics and possibly frying some of my servos. I almost haven't had time to play with them at all yet!

  10. #10
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    283

    Re: General Grievous

    4S LiPo works if you have a well-functioning gait, but not great for initial development or any other time when collisions or falls are likely. Even when the gait is working well, it does not hurt to have proportional torque limits (decrease maximum torque limit at higher voltage to get a consistent 'maximum' at all battery voltages) and fall/collision protections (e.g. if the IMU detects a fall, immediately disable torque to all servos to protect them from damage).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. General advice for a good starting kit
    By badpanda in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 07-16-2012, 02:53 AM
  2. general question on real time control and continuous motion
    By animaniac in forum Software and Programming
    Replies: 1
    Last Post: 10-17-2011, 04:43 PM
  3. Bioloid General I/O Board
    By JonHylands in forum Humanoids, Walkers & Crawlers
    Replies: 45
    Last Post: 01-11-2011, 08:27 AM
  4. Micro LCD for general use
    By jrowe47 in forum Mechanics / Construction
    Replies: 1
    Last Post: 02-04-2008, 10:47 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •