Most cell phones or laptops do not actually catch on fire.Now, for parallell powering, since I'm gonna use LiPo batteries, wouldn't that cause an issue if I try to charge two 2s batteries connected in series with my 12v power supply? My impression is that LiPo's are somewhat unstable and should be removed and charged separately under close supervision. This is a issue that I've been very unsure on how to deal with in the best way, so any input here is highly appreciated
It is true that, when you get it wrong with Lithium batteries, they do spectacularly catch on fire.
It is also true that, some things that you could do on other batteries (recharge after deep discharge, for example) count as punishing on Lithium batteries.
However, Lithium batteries are a fine technology, and when treated alright, do not actually spotaneously combust.
Most of the horror stories come from:
- people who think Lithium batteries work like NiHM
- people who think Lithium batteries work like Lead-Acid
- people who got bad batteries from the factory
- people who made mistakes and didn't catch themselves
You can charge a lithium battery with two wires, and it won't immediately catch on fire. However, as the battery goes through charge/discharge cycles, the internal resistance in each cell ("S") will slowly diverge, leading to one cell getting more charge than the other. Therefore, it's useful to make sure you do a balance charge at least once in a while (say, every 10 cycles.)
In order that you don't forget, it's totally OK to do a balance charge every time, too.
You can charge a lithium battery pretty fast (at several "C" rate) as long as you make sure it doesn't heat up too much. Slightly warm is OK. Uncomfortable to the touch is not OK. If you charge too fast, too often, you will wear the battery down faster. If you charge WAY too fast, see above about "punishing lipos" and spectacular fires.
You can NOT recover a lithium battery after it's discharged below 3.0V/cell or so (maybe 2.8V.) The batteries go through a very specific conditioning cycle in the factory to go from 0.0V to full charge, and that cycle actually builds up the oxide layer between the parts of the battery, that makes it actually work. Once you discharge the battery too far, you've irrecoverably damaged this oxide layer. If you somehow manage to "miraculously" "recover" an over-discharged battery from the borderlands, then you will have a battery with worse performance, higher internal resistance, more likely to build up heat, and less able to hold a charge. Use an undervoltage detector/cut-off at all times. (Took me two lost batteries to learn this!)
You're not supposed to "keep charging" a LiPo battery at full charge, because at the top voltage, the trickle through the internal leakage of the battery builds on to the oxide layer, slowly wearing the battery out. "floating" a battery at below-top charge, is supposed to be less damaging. Some electric car batteries try to keep the pack at 4.05V, for example. When I float, I typically do it at 3.9V-4.0V per cell, and it works OK. I have a LiFePO4 pack that I've done this to for four years (at 3.5V/cell) and it's still going strong. It does need rebalancing at times, though.
Do not parallel a 2S with a 12V supply, though; that would cause a house fire. 2S need <= 8V for parallel.
Regarding step-up versus step-down, it's a question of current capacity. The computer will likely draw 3-5A/19V fairly continuously. A step-up converter with 6A capacity will easily be able to meet the needs of the computer. Meanwhile, all of the servos will draw about 1A/12V when idle, but may draw 20A/12V when working hard. Thus, you'd need a much beefier step-down converter to feed the servos, if you set your battery pack at 19V. Also, I agree that NUCs are super finicky about input voltage, I had one (Zotac, AMD based) that only worked with 18.5V-19.5V input range, and no battery pack stays in that range, so it needed a regulator no matter what. The MX-64 will be OK with 10V-16V actual input voltage. You can also turn off the over-voltage alarm for those times when your 4S cell reaches the full 16.8V. That being said, I highly recommend 3S LiPo or 4S LiFePO4 for the reasons Tician suggest. I burned several MX-64 motors at 4S when they moved into interference because of software bugs, and the built-in over-heat protection wasn't fast enough to save them.
With Onyx X, I went 4S, because I had more of an idea what I was doing, and I started out simulating the software in a custom C++ rig on Windows, and when I finally ran on the bot, I ran with a 20% "Max Torque" limit while holding the bot in the air. I still managed to stall one servo at full power one time, but was sufficiently aware that I immediately (within a second) hit the power switch and the servo seems OK.
Bookmarks