Results 1 to 4 of 4

Thread: 4 dof ik

  1. 4 dof ik

    Hi all..

    I am trying to add a 4th DOF to my legged robot. I have managed to find and prove IK that works if the last part of the leg (Tarsus) remains vertical.

    Please see this image and spreadsheet.
    Click image for larger version. 

Name:	IK.jpg 
Views:	235 
Size:	66.2 KB 
ID:	6934

    Links to Image and Spreadsheet.
    https://drive.google.com/file/d/0B8l...ew?usp=sharing
    https://drive.google.com/file/d/0B8l...ew?usp=sharing


    What i want though is for the last part of the leg to vary it's angle to allow the legs to reach further and also be more flexible. I can see that Zenta has achieved this in the Phoenix code, but i don't understand his code.

    Any help much appreciated.


    Thanks
    Martin
    Last edited by mturneruk; 04-01-2017 at 03:30 AM.

  2. #2

    Re: 4 dof ik

    You cannot, in general, make the fourth axis always vertical, and still get three degrees of freedom in positioning.
    You need five independent degrees of freedom in your armature to get three degrees of position and two degrees of angle.
    At that point, the leg will still pivot when walking, but otherwise the contact point can remain at a position and stay vertical.

    Unfortunately, the image you linked to requires forum registration and login on some other forum, where I'm not a member, so I can't tell you much more than that.

  3. Re: 4 dof ik

    Sorry about that. I have fixed the image and also put a link to my spreadsheet with the workings.

    My project is this Quadruped.
    https://www.youtube.com/watch?v=jWKsVjQuVpQ`

    Here is a robot that has IK that allows the tarsus to vary its angle. (Phoneix Code).
    https://www.youtube.com/watch?v=RgV6BoCdTcc
    Last edited by mturneruk; 04-01-2017 at 03:38 AM.

  4. #4

    Re: 4 dof ik

    Yes, I am familiar with quadrupeds!

    Neither of the robots you link to keep the tarsus always vertical when moving the legs.

    What, specifically, is your question? The Phoenix code isn't terribly bad (although I personally think the particular indentation style is not easy to read) so if you could ask a specific question, I'm sure that someone could attempt to give a specific answer!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •