Results 1 to 3 of 3

Thread: Problems with Scorpion Mini

  1. Problems with Scorpion Mini

    I am having a problem getting the Scorpion Mini to output any voltage other than zero to the maxon motor I am controlling. The + and - battery connections on the Scorpion Mini are wired to a 5V regulator and the PWM input signal line is wired to a r/c receiver with a separate receiver battery. I have verified that the r/c receiver is correctly sending the PWM signals to the Scorpion Mini and the Scorpion Mini is correctly receiving the 5V power supply. Additionally, the LEDs on the Scorpion Mini operate correctly when I move the stick on the r/c transmitter (i.e. the red LED is steady lit when I move the stick left and becomes brighter as the stick is moved farther left and the green LED operates the same when the r/c transmitter stick is moved to the right. Also, both LEDs are off when the stick is centered). The motor is a 5V motor and only pulls a maximum of 1.9 Amps when started. Any suggestions to fix this problem?

    Thank you.

  2. Re: Problems with Scorpion Mini

    Well, you've already answered most of the tech support questions I would have asked you, but I've still got some general troubleshooting stuff for you to try, just to be sure. If you installed the screw terminal, try reflowing the solder on the header's pins to make sure you don't have any bad joints. For good measure, visually check the rest of the solder joints on the board to make sure there aren't any bridged pins on the microcontroller or the drive chip. Also verify that your motor works with another controller or a battery.

  3. Re: Problems with Scorpion Mini

    Well, I found out what the problem was. On each of the two Scorpion Mini boards I tested, the logic on the board seems to work fine at 5V (that is probably the reason the LEDs were working correctly). However the board does not supply any power to the motor until it has at least a 5.4V supply. I switched the power to a 6V regulator and the system works fine now. Thank you for the suggestions.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Scorpion Mini question(s)
    By xyzzy1126 in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 02-21-2007, 04:26 PM
  2. Problems with Probing Robot
    By Bushwhackr in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 01-31-2007, 09:35 PM
  3. Problems linking to libphidget21
    By bidi in forum Software and Programming
    Replies: 3
    Last Post: 01-31-2007, 10:11 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •