Results 1 to 6 of 6

Thread: Fluid Pressure Sensor

  1. #1
    Join Date
    Mar 2017
    Location
    Planet Earth
    Posts
    10
    Rep Power
    11

    Fluid Pressure Sensor

    I am a bit stuck in another project on how to measure fluid pressure electronically. I cant seem to find any sensors online for it. I was thinking about using a pushrod with a spring on the end and then a force sensor. But i feel that this will be full of inaccuracy. Are there any fluid pressure sensors that can interface with arduino and if so what is their price range?


    Thank you very much

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,314
    Images
    27
    Rep Power
    279

    Re: Fluid Pressure Sensor

    I am assuming you meant liquid, since there are plenty of gas pressure sensors available for arduino (cheap SMD altimeters). Search digikey for pressure sensors with a maximum operating pressure greater than 300kPa and you will find many sensors capable of handling liquids. Which liquids are safe to use with the sensor depends on the membrane isolating the sensor element, so have to read the datasheet and maybe contact the manufacturer if directed by the datasheet. Most of the less expensive sensors provide only a small ~100mV output that requires external amplification and temperature compensation, but slightly more expensive versions include all of the amplification and conditioning within the sensor.
    Last edited by tician; 04-04-2017 at 11:05 AM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3
    Join Date
    Mar 2017
    Location
    Planet Earth
    Posts
    10
    Rep Power
    11

    Re: Fluid Pressure Sensor

    Oops, clicked the wrong reply button the first time. Original message:
    "Thank you very much, that was very helpful. Now for calibrating the sensor, can i use air with an inline mechanical pressure gauge to develop my calibration curve or will that membrane prevent this from working due to compressibility or density?"

  4. #4

    Re: Fluid Pressure Sensor

    Pressure is pressure, so in general, the compressibility and density response would be the same between fluids and gasses. (Note: college physics recollection here; I haven't dealt with these sensors in forever!)
    The main problem as I recall would be if your membrane is permeable to gas but not fluid, in which case the pressure would leak out. You have to check the data sheet for the sensor you get for specifics.
    In general, manufacturer's data sheets are a glorious source of information about gadgets and widgets you use!

  5. #5
    Join Date
    Mar 2017
    Location
    Planet Earth
    Posts
    10
    Rep Power
    11

    Re: Fluid Pressure Sensor

    Thats what i was wondering, if the membrane messes up the ability to measure pressure since air can compress and slip through smaller holes

  6. #6
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,314
    Images
    27
    Rep Power
    279

    Re: Fluid Pressure Sensor

    If there is any internal electronics in the sensor, then it is very like that it has been tested and calibrated at the factory using dry air.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) How to design a pressure sensor squeeze ball?
    By anurooppv in forum Sensors
    Replies: 0
    Last Post: 01-28-2015, 01:34 AM
  2. Question(s) How pressure sensor and MBED works?
    By KAYSHEHU in forum Sensors
    Replies: 2
    Last Post: 07-05-2012, 04:42 AM
  3. Sensor required for pressure distribution on seats
    By skumar_m226 in forum Sensors
    Replies: 2
    Last Post: 02-22-2012, 08:36 AM
  4. Discussion : Making phoenix's motion fluid
    By gonzo in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 03-04-2011, 06:38 AM
  5. Question(s) Sensors , Hitec Robonova Distance Sensor and Ultrasonic sensor
    By BrandonG32 in forum Sensors
    Replies: 1
    Last Post: 08-18-2008, 11:07 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •