Results 1 to 4 of 4

Thread: WheelChair Motor help

  1. #1

    WheelChair Motor help

    Hi their Guys and Gals,
    I am new to the Robot building world. I have been playing with RC cars and Quads for years now am want to build a Rover.
    I have been looking just about everywhere I can find on the web, but I can’t for love nor money find a connector to build off for my Wheelchair motors. I want to connect them to pneumatic sack truck wheels. I do not want to use a chain system as this I will be taking the completed project around schools to promote coding, don’t want to break any fingers.

    Can anyone help or provide some links for a connector for the P6001415 Invacare motor




    Thanks

  2. #2

    Re: WheelChair Motor help

    A picture of the motor doesn't help, unless it includes the output shaft, and also some kind of scale so we can tell how big the shaft is.

    In general, when it comes to adapters and hubs, if the output shaft has a milled flat, you might be able to find something that fits. If the shaft has a spline of some sort ("teeth") then you have to go to the manufacturer to find something that fits, or adapt whatever came with the motor (i e, if there are existing wheels/hubs.)

    If neither of those options work out, then you're going to have to make some of your own, or perhaps order some parts made. If you don't have access to and know how to use a lathe or milling machine, that becomes expensive!

    Now, if your tires have a specific hub size, too, we'd of course also need to know the mounting type of that hub. Bolt pattern? Round hole with pins? Square hole?

  3. #3

    Re: WheelChair Motor help

    Hi there, this is solved.

    I bought the wheels to go with the motor, removed the hubs and added to new set of wheels.

    Thanks

  4. #4

    Re: WheelChair Motor help

    Glad you got it working! Factory parts intended to fit are usually the safest bet :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) wheelchair motor : removal of wheel hub
    By anilkumar15 in forum Robotics General Discussion
    Replies: 1
    Last Post: 09-08-2016, 03:02 PM
  2. Question(s) Motor Controller for wheelchair motors
    By DangerousThing in forum Power
    Replies: 1
    Last Post: 04-18-2014, 10:31 PM
  3. Question(s) Alternative to wheelchair motor for payload of 50kg/110lbs
    By garagelane in forum DYNAMIXEL & Robot Actuators
    Replies: 13
    Last Post: 04-11-2014, 01:26 AM
  4. Wheelchair motor control
    By yadusahron in forum Off Topic
    Replies: 3
    Last Post: 04-10-2014, 11:54 PM
  5. Question(s) 24v Wheelchair Motor Wiring Question... HELP!!
    By prosper50 in forum Robotics General Discussion
    Replies: 16
    Last Post: 04-15-2012, 02:21 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •