Results 1 to 7 of 7

Thread: Beta testing XL430

  1. #1
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    81

    Beta testing XL430

    Hi,

    On Facebook I noticed that Robotis was calling for beta testers for their upcoming XL430 servos. I thought that would be interesting and gave them a post and an application form. So after a couple of weeks I got 3 of the new XL430 on my door.

    Click image for larger version. 

Name:	XL430_3-sides.jpg 
Views:	232 
Size:	75.9 KB 
ID:	6968

    Take a look at this Preliminary Product document for all the available specs. I believe these servos are going to be pretty popular. I'm not sure about the cost (they do say low cost), maybe somewhere between the AX-12 and AX-18?
    But compared to the AX-12 and AX-18 the specs are superior.

    Some points to mention.

    • Contactless absolute encoder (12BIT,360 deg!)
    • Smaller formfactor than the AX-12/18, about same torque/speed as the AX-12
    • Protocol 2 with all the new features
    • TTL Async bus up to 4.5 Mbps
    • 4 Different operation modes
    • Real PID
    • Different velocity profiles
    • Secondary shadow ID and much more


    A picture of the content of one servo-box:
    Click image for larger version. 

Name:	XL430_Complete-box.jpg 
Views:	217 
Size:	75.3 KB 
ID:	6967
    Very useful that it comes with a cable with the new and the old connector. For testing I connected one servo to the USB2AX and using their R+ manager 2.0. Watch my instagram for short test vids of it moving.

    A couple of pics compared to AX-12/18:
    Click image for larger version. 

Name:	XL430vsAX18_frontview.jpg 
Views:	241 
Size:	66.6 KB 
ID:	6964

    Click image for larger version. 

Name:	XL430vsAX18_sideview.jpg 
Views:	208 
Size:	54.5 KB 
ID:	6965

    When it comes to the mounting holes there are some cons and pros. On the bottom and both sides there are 4 mounting holes that are 4mm deep and a diameter of 2.1mm. On the top and front there are only two holes. But you can use the case screws on the front side too (look at the document). But I'm not sure if I like that the hole isn't metal tapped, only based on selftapping screws. In the long term this isn't a good solution.

    I really like the relative narrow depth of the servo. I measured the depth (distance between the front and rear horn) to be about 37.80mm. The manual says 34mm, but that's only the servo case. For a legged robot this is good news.
    Click image for larger version. 

Name:	XL430_Depth.jpg 
Views:	187 
Size:	77.4 KB 
ID:	6966

    If you are interested in other dimensions let me know. The horn has a diameter of 20.35mm, the 4 mounting holes on the horn is metal tapped and matches the AX-12/18 pattern.

    Their solution for the rear free-horn is simply ingenious. I love that you can guide the wire through the horn and it give a good solution for avoiding to much twist and movement of the wire during movement.

    I must say I love the increased resolution and full 360 travel. Especially their extended position control mode (multi turn) that gives you an exact position range of
    -1,048,575 ~ 1,048,575 !
    I can imagine letting the servo drive a large gear for more torque on a legged robot.

    I'll do some more testing and hope to get time posting more info. Maybe taking one apart?

    Btw, I'm wondering if someone has already written a new Protocol 2.0 library? I thought I should give it a try on one of my Teensy's too.

    Oh, I'm not sure if you know that the MX servos can be updated to the Protocol 2?


    Having fun.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  2. #2
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    81

    Re: Beta testing XL430

    Some text got lost in my first post. Imagine using this servo as a linear actuator and let the servo drive a ball-screw with exact position control and lots of torque.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  3. #3

    Re: Beta testing XL430

    Ah! I've been waiting for a non-wheel version of the MX-12W. I guess this is what happened instead :-)
    Thank you for sharing and writing this up.

    If "low cost" means they're benchmarking against the XM and XH series, that'd be like a hundred bucks.
    If "low cost" means they're a replacement for the AX-12A, then that's great!

    Plastic gears, smaller connector, and self-tapping mounting holes sounds like they're aiming for the latter, though, so there is hope!

  4. #4
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    81

    Re: Beta testing XL430

    Quote Originally Posted by jwatte View Post
    If "low cost" means they're a replacement for the AX-12A, then that's great!
    That's my impression. The noise of the gears sounds a bit "cheap". I do think it will be a little more expensive than the AX-12 due to the encoder. I do also hope they will release several alternatives with more torque/speed. In their survey they asked if a metal gear version would be interesting..
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  5. #5

    Re: Beta testing XL430

    I do also hope they will release several alternatives with more torque/speed.
    isn't that what the XM 430 is?

  6. #6
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    81

    Re: Beta testing XL430

    Lol. I didn't realize that the XM430 had the same size.. Even better. I probably have to try some of them too one day.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  7. #7

    Re: Beta testing XL430

    I haven't seen the width/height measurements, but the thickness (horn to horn) seems very similar.
    It'll be interesting to see if these are similar in the AX-12/AX-18 senseo, or similar in the MX-28/MX-64 sense!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Testing the MX-64T and MX-106T
    By Zenta in forum DYNAMIXEL & Robot Actuators
    Replies: 33
    Last Post: 11-13-2017, 02:20 AM
  2. First impressions testing the new XL-320 Robotis Dynamixel
    By siempre.aprendiendo in forum Robotics General Discussion
    Replies: 0
    Last Post: 03-16-2014, 12:20 PM
  3. AX-12 Electrial Efficiency testing
    By sarendt in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 03-13-2011, 11:46 AM
  4. Stress testing and debugging AX-12+ servos
    By Pi Robot in forum DYNAMIXEL & Robot Actuators
    Replies: 24
    Last Post: 01-16-2011, 02:14 PM
  5. Virtual Testing
    By Firestorm65 in forum Mech Warfare
    Replies: 5
    Last Post: 02-21-2009, 11:45 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •