robotics company robot company  

Go Back   Trossen Robotics Community > Robotics > Project Showcase

Project Showcase Have a project that you're dying to pimp? It doesn't matter if it involves robotics, RFID, HCI, or what, as long as you think it's cool, pimp it here! Need more space for pics/videos email us:)

» Navigation Menu
Homepage
Forums
TRC Tutorials
Member Blogs
Data Center
Image Galleries
Links Directory
Contact Us

Shop Robotics
» Introduction Tutorials

» November 2009
S M T W T F S
1 2 3 4 5 6 7
8 9 10 11 12 13 14
15 16 17 18 19 20 21
22 23 24 25 26 27 28
29 30 12345
» Current Poll
Are you going to use Nerf-style weapons at the next Mech-Warfare?
Yes. - 18.75%
3 Votes
No. - 68.75%
11 Votes
Yes, but only if double damage is allowed. - 12.50%
2 Votes
Total Votes: 16
You may not vote on this poll.
» Trossen Robotics Blog
Phoenix 2.0 Software Released...
HUV Robotics Bioloid Accessories are bac...
The Quads are Coming!...
Just in time for Halloween!...
Boston Dynamics does it again...
» Join Us Elsewhere!






» Online Users: 209
3 members and 206 guests
Rick Brooks, siempre.aprendiendo, Zenta
Most users ever online was 1,301, 09-11-2009 at 06:59 PM.
» Stats
Members: 3,244
Threads: 2,329
Posts: 31,356
Top Poster: Adrenalynn (5,122)
Welcome to our newest member, whinolandres
Reply
 
Thread Tools Search this Thread Display Modes
  #1  
Old 08-17-2007
jonathanuwguy
jonathanuwguy is offline
Abacus
 
Join Date: Aug 2007
Posts: 2
Rep Power: 0
jonathanuwguy is on a distinguished road
2nd Place The officebot



the "officebot" is not the official name of the robot. I called it so because it's a robot that can run around the office talking to people, playing sounds and music and even shooting rocket at them.

Here are the main features of the robot:

• Fully controlled through computer with client and server components.
• Full audio and video conference capabilities.
• 24/7 availability.
• Remote charging and maintenance.
• All wheel drive.
• Remotely controlled rocket launcher system.
• Text-to-Speech and voice recognition.
• Remote sounds and music.
• Variable speeds.

Here is a picture of the robot:




For complete details on specs, part, costs, journal, pictures and videos:

http://www.techconsultants.us/officebot

-----------------------------------------------------------------------

About officebot:

The officebot idea came to me when I was sitting in a coffee shop working. I wanted to have something so I could go into a meeting and join it remotely. This idea expanded and eventually we have a 4 wheel drive robot that can be controlled by anybody anywhere as long as they have a connection to the office's network. The robot can be remotely driven at anytime without any direct local intervention thanks to the remote docking system that allows the robot to be docked and charged remotely. The coverage area of the robot is limited only by the coverage of the wifi system in the office (It can roaming freely anywhere in our 20000sqft office). Dual gateway wireless systems with high gain antennas provide stable and strong main wireless connection and backup peer-to-peer connection (in case the main wireless connection is lost). The high resolution camera with builtin array microphone technology and strong speakers provide complete video and audio chat solution at standard conference quality. The robot is equipped with a rocket launcher system to allow remote operator to send clear warning to a co-worker for sending work request to him or her without his or her approval. This robot is also equipped with headlight system to allow night driving and night patrolling of the office for unwanted visitors such as rats or raccoons (our office floor is in a downtown high rise so these probably don't exist but you never know .

The brain of the robot is a strong centrino dell laptop that hosts server application which allows remote operator to control all functions of the robot: driving at various speeds, doing voice and video chat, shooting rockets, control light and camera pan, tilt base, sneaking up on a sleepy coworker and playing loud and annoying sounds or music or maybe commanding the robot to speak some phrases from your text using an male or female voice.

Multiple video encoding settings allow the system to be optimized for bandwidth to allow remote access from public wireless places such as coffee shops.


For video demos of the robot, cam view, docking view, voice, audio, cam, rocket launchers, lights, control software, etc.., see the website mentioned above. Please let me know if the clips are not viewable with some players so I can provide different formats.

Cheers,
Jonathan

Last edited by Dave; 09-07-2007 at 06:51 PM. Reason: 2nd is almost as good as first!
Reply With Quote
  #2  
Old 08-22-2007
Alex's Avatar
Alex
Alex is offline
trbothead - TRC admin
 
Join Date: Sep 2006
Location: Carol Stream, Illinois
Posts: 1,677
Blog Entries: 8
Images: 118
Rep Power: 75
Alex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant futureAlex has a brilliant future
Re: The officebot

Pretty sweet project Jonathan! I bet that's a load of fun to drive around.

Thanks for the submission
__________________

“In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed”
- Charles Darwin

New to the TRC?
Customize Your Profile -- Post To and Customize Your Blog -- Create Your Own Photo Album -- Create a Tutorial
Reply With Quote
  #3  
Old 09-08-2007
jonathanuwguy
jonathanuwguy is offline
Abacus
 
Join Date: Aug 2007
Posts: 2
Rep Power: 0
jonathanuwguy is on a distinguished road
Re: The officebot

Woohoo! Thanks guys!
Reply With Quote
Reply

Bookmarks


Currently Active Users Viewing This Thread: 1 (0 members and 1 guests)
 
Thread Tools Search this Thread
Search this Thread:

Advanced Search
Display Modes

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is Off

Forum Jump

Powered by vBadvanced CMPS v3.2.0

All times are GMT -5. The time now is 05:23 AM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.