robotics company robot company  

Go Back   Trossen Robotics Community > Robotics > Robotics General Discussion

Robotics General Discussion Have something to discuss, but there's not a forum for it below?

» Navigation Menu
Homepage
Forums
TRC Tutorials
Member Blogs
Data Center
Image Galleries
Links Directory
Contact Us

Shop Robotics
» Join our Chatroom!


You'll need an IRC Client
» Introduction Tutorials

» Robot Parts!
» TRC On Facebook!
» Arbotix
» RoboGames
» Data Center Entries
MECH_Puppeteer.zip
By Droid Works
04-20-2008 06:24 PM
cm-5.pdf
By trey3670
08-21-2008 11:51 PM
Default RoboBuilder...
By Alex
10-28-2008 10:43 AM
CM-2 Manual(english)
By Alex
07-28-2008 10:44 AM
Strabo Pathfinder
By Matt
05-08-2008 04:09 PM
» ComBots
» Turrets!
» Trossen Robotics Blog
DIY Vacuum Forming!...
Trossen Robotics DIY Project Contest...
Like Us! Like Us!...
Interlink FSRs now with Female Connector...
InterbotiX Robot Turrets...
» Join Us Elsewhere!






» Bioloid Premium Kit
» Online Users: 363
12 members and 351 guests
elios, kanda, mallster, mikaela55, Psykoman, Rick Brooks, robotbill, sthmck, TeamThinkTank, Tyberius, Zenta
Most users ever online was 1,301, 09-11-2009 at 05:59 PM.
» Stats
Members: 4,307
Threads: 2,915
Posts: 37,356
Top Poster: Adrenalynn (5,329)
Welcome to our newest member, mikaela55
Reply
 
Thread Tools Search this Thread Display Modes
  #1  
Old 09-29-2007
vignetting
vignetting is offline
Abacus
 
Join Date: Sep 2007
Posts: 1
Rep Power: 0
vignetting is on a distinguished road
Smile Computer controlled Motor?

Hello everyone,

I never made a robot or such thing. So I have no idea about everything, I mean mostly.
And I'm trying to build a rotating cylinder with some small screens in side. In fact, it is a zoetrope with screens inside.

Anyway, I had a hard time to find a thing to connect all the wires to the rotational structure from the base. and I found thing called slip ring by the moog or the mercotac company. So one issue is down.

Another thing is a motor. I don't know what kind I should get. I think it's going to be about 14 inches (diameter) and 8~7 inches(height) probably wood. So it's not that heavy and drive it less than 1000 rpm?

The major issue is that I want it to control the rpm of motor by computer(usb or serial connection).

1. What kind of motor do I want?
2. How can I connect the motor to computer in order to control the rpm?

It would be great if anyone can recommend specific parts for this.
Thanks a lot and have a great weekend~
Reply With Quote
  #2  
Old 10-01-2007
Matt's Avatar
Matt
Matt is offline
Robonerd Wrangler
 
Join Date: Sep 2006
Location: Chicago Illinois
Posts: 663
Images: 7
Rep Power: 53
Matt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant futureMatt has a brilliant future
Re: Computer controlled Motor?

Hello,

To control a motor from a computer you want to use a Servo controller to output a PWM signal to a DC motor controller. See the graphic and description on this page. There are a whole line of motors from banebots that have many different RPMs. You should be able to find a motor to match your needs there.
__________________
Matt Trossen - Say hello on the introduce yourself thread!
Reply With Quote
Reply

Bookmarks


Currently Active Users Viewing This Thread: 1 (0 members and 1 guests)
 
Thread Tools Search this Thread
Search this Thread:

Advanced Search
Display Modes

Posting Rules
You may not post new threads
You may not post replies
You may not post attachments
You may not edit your posts

BB code is On
Smilies are On
[IMG] code is On
HTML code is Off

Forum Jump

Similar Threads
Thread Thread Starter Forum Replies Last Post
Question(s) fixing Colson wheels on motor shaft stefano.antonelli Mechanics / Construction 6 02-12-2008 11:37 PM
Contest Entry Fuel Burner Control System BillW Project Showcase 4 08-03-2007 03:54 PM
Fast Spinning DC Motor + Controller BillW Actuators 3 06-29-2007 03:12 PM
Phidget controlled Gun Turret defends home Vaughn I/O Boards and Controllers 1 06-15-2007 04:04 PM
Controlling a MAXI Motor Controller shobley I/O Boards and Controllers 2 02-02-2007 12:59 PM

Powered by vBadvanced CMPS v3.2.0

All times are GMT -5. The time now is 02:43 AM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2010, Jelsoft Enterprises Ltd.