robotics company robot company  

Go Back   Trossen Robotics Community > Community Tutorials > Build Articles

Home Submit Tutorial What's New What's Popular Search

T-1 Rise of the Machines (Page 5)
Old 11-18-2008 03:12 AM
4mem8
4mem8 is offline
T-1000
 
Category: Build Articles
Views: 5,419
Replies: 1
Send a message via AIM to 4mem8
Difficulty: Very difficult
Estimated Time: Unknown at this time
Skills Required: Modeling, Metal work, soldering, Electronics,Engineering,co-ordination,Programming [argh], Weapons systems [GWJax],
Parts Required: Tracks, Lexan or Polycarb sheet, SES brackets, HRS 5990t servos, Fiber glass components, Cardboard, Balsa wood, MDF, Cyno glue, MDF sanding sealer, Duratek, Carbon cloth,Modeling clay,Electronic components,Hitec servo tester, 3 NiMh Batteries, ITX M/B, 60W P/S, Solid state Hdd,
Switches, LEDs, Two Gattling guns, Camera, communication system,2 12v 50:1 DC motors,Rotational base bearing[ local machine shop], 2 1/4 scale servos, Documentation of project,
Tools Required: Drill press, Lathe, scaling dividers, X-acto knife, drills, taps, pens, curved protractors, Straight edge, Bandsaw, Fret saw, Dremel, Fiber glassing tools, cordless drill, Allen keys, Small spanners, Pliers, Square,
T-1 Rise of the Machines Part 5



T-1 Rise of the Machines





These sections are for the raised neck area which will be back filled for a radius.




As you can see we now have all the neck sections glued in place.




Lower radius now refilled to a larger radius and the neck area also filled.




Close up of neck area.




Rear neck area being built up with balsa wood.




Rear side angle shot showing the complex curve.




Profile curves for the radius back filling, Note the beveled front edge, Critical for a smooth finish.




Rear has now been radiused.





Starting to take shape now.




Take away the MDF supports and you can see that it is getting close to the required shape.




Front/side view.




Fitting the bottom in place.




This is the area where the rotational bearing will go. Has to have a 10mm spacer under the alloy ring.




Other half of the rotational bearing plate on the main body. This area will be fiber glass or carbon when cast.





10mm balsa spacer, this will be cast into the fiber glass mold




Alloy bearing plate on top of spacer..




Disc on the end is for the spring system.




Another angle of the disc.

Seeing that we are getting close to the molding process here is a list of items that we require to make the plugs and molds for the two main bodies.

Products that will be used are:
[1] Polyester resin for the mold
[2] Fiber glass tissue: First lay up after the gelcoat.
[3] 200g chopped strand matt: Second lay up after the tissue.
[4] 400g chopped strand matt: Third lay up after the 200g Matt.
[5] Release wax: used to polish the mold and prior to laying up.
[6] Release agent: PVA based liquid so glass does not stick to mold.
[7] Gelcoat: Used in the first coat in the lay up.
[8] Plastiscine: filling in gaps when making the box to hold the mold.
[9] MDF fiber board: Making jigs to hold the plug.
[10] Polyester thinners or acetone: Washing brushes and thinning.
[11] Duratek: Used for spraying into the mold then lay up, to get a smooth gray finish, Also used for the final finish on plugs.





Upper and lower body plugs have now been primed with a sandable laquer filler.





MDF box for holding the upper body shell, The upper body is placed on it's side in the box.





These MDF supports will fit around the upper body shell.




Upper body plug in the box ready for the MDF supports.




Notice that the MDF supports are as close as you can get them against the body, These will support the 3mm mdf which will be contured against the body plug, This is to form a platform to which the fiber glass will be laid on to form a flange.




Bottom view of upper body plug.




Larger MDF box for the lower body plug. The same process will occour as for the upper body plug.




Lower body plug, with supports ready for the 3mm MDF platform.











This is all I have to date, more pics when i have done some more work, This project could take up to another two months or more as there is a lot of work ahead yet to be done.
[/center]
[/left]
[/center]
[/left]
[/center]

[/left]
[/center]
(Page 5 of 5)
__________________
People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.

Tags: None



Replies to Tutorial: T-1 Rise of the Machines
  #1   Report Post  
Old 02-15-2010
4mem8's Avatar
4mem8
4mem8 is offline
T-1000
 
Join Date: Apr 2008
Location: Nelson, New Zealand
Posts: 1,320
4mem8 4mem8 4mem8 4mem8
Send a message via AIM to 4mem8
Re: T-1 Rise of the Machines

So sorry this project is taking so long. Have been out of work now for so long and funds dried up. but i am trying to restart it. [hate leaving a project unfinished] so i will try to do some work on it abeit a bit slow. i know a few of u were following this project so will do my best.
__________________
People yearn after this robotic dream, but you can't strip your life of all meaning, emotion and feeling and expect to function.


 


All times are GMT -5. The time now is 12:38 PM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2010, Jelsoft Enterprises Ltd.