robotics company robot company  

Go Back   Trossen Robotics Community > Community Tutorials > Mod, Hack

Home Submit Tutorial What's New What's Popular Search

Control Your Robot with an iPhone
Old 06-27-2009 09:00 PM
mannyr7
mannyr7 is offline
Neuron
 
Category: Mod, Hack
Views: 1,063
Replies: 0
Send a message via Yahoo to mannyr7
Difficulty: Easy
Estimated Time: 10 minutes
Skills Required: Basic PC skills
Parts Required: 802.11 wifi network
Apple iPhone or iPod Touch
A PC running Windows XP, Vista, or OS X. Beta for Ubuntu Linux available as well.
Tools Required: Software. Ok, for this tutorial, we are going to get Clyde moving via iPhone. I use Lynxmotion's Visual Sequencer SEQ-1 linked to Clyde via Bluetooth, but this hack will work for any bot that can be controlled via PC software-based keyboard input. Essential to this hack is a lttle piece of software called Wifi Pad. This actually consists of a server app which runs on your control pc and remote wifi client app you download from the Apple App store onto your iPhone. It was intended to be a substitute to an actual gamepad for playing your computer games.
1. Install WifiPad on your iPhone from the Apple App Store..

2. Install the WifiPad server app from http://wifipad.com onto your PC. Assigning a server name is optional, or you can connect using IP address later. Now is a good time though, using ipconfig.exe to find out your host PC's address on your local net. Click on the WifiPad Server app's D-pad and buttons and assign them some keys on your PC keyboard you'd like to control your bot. (direction arrows, num 1-9, W,A,S,D, whatever...)




3.
You'll have to enable a couple ports on your firewall to allow your PC to communicate with the iPhone. Under Windows Firewall settings, Uncheck "Do Not Allow Exceptions", if it is checked. Then, on the "Exceptions" tab, create ports for UDP 8989, TCP 8989 and UDP 8990. I recommend you use the "Change Scope" button to only allow access to your local subnet.




4. Configure whatever software you use to move your bot to respond to keyboard input. I use Lynxmotion's Visual SEQ.





5. I'll open the 'Advanced Play' module in SEQ and map some sequences to my cursor keys (UP, DOWN, LEFT and RIGHT) and the spacebar.





6. Ensuring you have wifi enabled on your iPhone, launch WifiPad. It should scan the network and find your WifiPad server. Alternatively, connect using the IP address of the host PC you have WifiPad server installed on.


7. Have fun!


Tags: mannyr7 clyde iphone wifi gamepad




 


All times are GMT -5. The time now is 06:00 AM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.